AXIS#.HOME.AUTOMOVE

Description

AXIS#.HOME.AUTOMOVE specifies whether the axis starts the configured homing move when the axis is enabled.


  • When Axis 2 is configured as a gantry (AXIS2.CMDSOURCE = 4), AXIS1.HOME.AUTOMOVE configures the automatic homing behavior for both Axis 1 and Axis 2. The drive ignores AXIS2.HOME.AUTOMOVE.
Value Description
0 The axis never starts a homing move when the axis is enabled.
1

The axis starts a homing move when the axis is enabled.

This homing move is skipped if:

The axis is already homed

The axis is not in position mode (AXIS#.OPMODE= 2)

The axis is not in service mode (AXIS#.CMDSOURCE= 0).

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 1

Default Value

0

Data Type

Integer

See Also

AXIS#.HOME.MODE
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
AXIS1.HOME.AUTOMOVE

5008h

04h

Unsigned8

-

-

Read/Write

No

AXIS2.HOME.AUTOMOVE

5108h

04h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.HOME.AUTOMOVE

6101

17D5

Unsigned8

Read/Write

-

AXIS2.HOME.AUTOMOVE

71637

117D

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.HOME.AUTOMOVE

6101

Unsigned8

Read/Write

-

Related Topics

Homing